Solution
Concrete Compression Testing
Testing the strength of concrete is essential for assessing the structural integrity and performance of concrete in various construction and infrastructure applications.
Testing the strength of concrete is essential for assessing the structural integrity and performance of concrete in various construction and infrastructure applications. A compression test is needed to ensure the concrete meets the specific strength requirements for structural use.
Interface suggests using the 1101 Compression-Only Ultra Precision LowProfile™ Load Cell in the compression test frame. A sample of concrete will be placed in the test frame, and the concrete will be compressed. The measurements from the compression test are recorded using the INF-USB3 Universal Serial Bus Single Channel PC Interface Module and logged when attached to the customer’s PC laptop or computer.
Interface’s 1101 Compression-Only Ultra Precision LowProfile™ Load Cell and paired instrumentation successfully measured and recorded the forces during the concrete compression test.
1101 Compression-Only Ultra Precision LowProfile™ Load Cell
INF-USB3 Universal Serial Bus Single Channel PC Interface Module with supplied software
Customer PC or Laptop
The 1101 Compression-Only Ultra Precision LowProfile™ Load Cell is installed into the compression test frame
A compression test is done onto a concrete sample. The 1101 Compression-Only Ultra Precision LowProfile™ Load Cell measures the forces of compression.
These measurements are recorded using the INF-USB3 Universal Serial Bus Single Channel PC Interface Module, which can be viewed and logged when attached to the customer’s PC laptop or computer.
Notifications